Legacy Conversion
If you are familiar with programming older, legacy 86100D instruments made before FlexDCA was introduced, you'll benefit greatly from this section. Click on the following links to locate tables of legacy 86100D commands that are matched to similar FlexDCA commands. Each legacy 86100D command subsystem is listed below. In many cases, there is not a one-to-one correspondence between legacy 86100D and FlexDCA commands. For some commands, the FlexDCA version may only provide a query form or, in the case of TDR/TDT mode, do not exist at all. Links in the table display information on the relevant FlexDCA command.
- Common Commands
- Root Level Commands
- :SYSTem Commands
- :ACQuire Commands
- :CALibrate Commands
- :CHANnel Commands
- :CRECovery Commands
- :DISK Commands
- :DISPlay Commands
- :FUNCtion Commands
- :HARDcopy Commands (FlexDCA does not support this subsystem at this time.)
- :HISTogram Commands
- :LTESt Commands
- :MARKer Commands
- :MTESt Commands
- :MEASure Commands
- :SPARameter Commands (FlexDCA TDR commands are not similar. Use the SCPI recorder to learn about commands for TDR mode.)
- :SPRocessing Commands
- :TDR Commands
- :TIMebase Commands
- :TRIGger Commands
- :WAVeform Commands
- :WMEMory Commands